Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV312 drive with a remote speed pot is working in reverse?
Issue:
Reversed remote speed pot on an ATV312 drive.

Product Line:
ATV312

Environment:
All serial numbers

Cause:
Potentiometer is working backwards

Resolution:
Swap the  +10vdc and the com terminal wires on the potentiometer to reverse the potentiometer operating direction.