Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between IL1R (Logic input real image) and IL1I (Logic input physical image) on the ATV Process Drives?
Issue:
Difference between IL1R (Logic input real image) and IL1I (Logic input physical image) on the ATV Process Drives

Product Line:
ATV600 ATV900

Environment:
All

Cause:
N/A

Resolution:
IL1R and IL1I could be different if we have to reverse the input state to do some operations, for example, we have DI2-high, and in order to activate an assignment, we must have DI2 low, So with DI2 high, the physical image here is 1 and the real image is 0). You can consider them as inputs and outputs of a logical circuitery (inputs = physical images ; outputs = real images). the outputs correspond to what we really apply to another circuitry to do other operations.
By the way, if we don't have to reverse any logical-input state (input state=output state), IL1R=IL1I (physical image = real image).