Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you run the motor in reverse on the ATV630 and ATV930 using Telegram 1 with the profinet option card?

Issue:
How do you run the motor in reverse on the ATV630 and ATV930 using Telegram 1 with the profinet option card VW3A3627?

Product Line:
ATV630 and ATV930  with the Profinet VW3A3627 option card.

Environment:
Telegram one only

Cause:
Wants to run the motor in reverse using telegram 1 in profinet.

Resolution:
You have to write a hex C000 which is negative -100% of the max freq tFr range and the motor will run in reverse
The frequency reference is normally the second word in the profinet output table for command.

Schneider Electric Nigeria

Attachment(s)
Telegram run motor in reverse.JPG.jpg [54.35 KB]