Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the acceptable input voltage range for Altivar 6xx and 9xx Process Drives?
Issue:
Acceptable input voltage range for Altivar Process Drives ATV630/930

Product Line:
Process Drive

Environment:
All

Cause:
Supply Line Voltage

Resolution:

The line voltage tolerance is +10% and -15%.

Per the ATV600 and ATV900 Catalog, the range is as follows:
- 200 - 15%...240 + 10% three-phase for ATV…M3
- 380 - 15%...480 + 10% three-phase for ATV…N4
- 500 - 15%…690 + 10% three-phase for ATV….Y