Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Incremental encoder (HTL) cable selection for connection to Altivar Process ATV930 variable speed drive
There is no specific requirement for encoder cable. For short distances (several meters) it is enough to buy 7x0.14mm2 shielded cable from a local producer/distributor.
But for big distances, bear in mind voltage drop. The instruction sheet of the dedicated encoder (example from ATV930 HTL encoder card VW3A3424 here below) shows minimum cross-section depending on encoder cable length and consumption.

Also check the encoder signals required by the encoder manufacturer whether 6 wires (A, nonA, B, nonB, Supply+, 0V) are enough.
For example 1XP8032-xxx Incremental HTL encoder from Siemens:
https://support.industry.siemens.com/cs/attachments/27102847/MA_IN_1XP8012_1XP8032-1xHTL.pdf?download=true

If the incremental encoder is equipped with a standard M23 connector (male), then it is also possible to buy a prewired cable + encoder connector (M23) from various local producers. Because Telemecanique sensors are no longer part of Schneider Electric, such cables are not in Schneider Electric's offer (In the past, there was for example XCCPM23121L5 offered by Schneider Electric).
I recommend searching on the web: "Pre-wired M23 female connector for incremental encoder, cable 5 m" and finding your manufacturer or distributor.

Schneider Electric Nigeria

Attachment(s)
QGH17640-00.jpg [114.2 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings