Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I obtain schematics for the AC Drive power board?
Issue:
Is there a way to obtain Schematics for a Schneider Electric AC Drive power board?

Product Line:
Altivar AC Drives, Process Drives

Environment:
All

Cause:
Repair

Resolution:
Drive Products Support does not provide that level of information to the public.  It is internal, proprietary information.  The Schneider Electric Repair Depot does board level repairs, however, typically smaller drives, repair is not very cost effective, and they should simply replaced if/when needed.
The Schneider Electric Repair Depot can be contacted by calling 800-950-9550, more information is available here: Contact Us - Schneider Electric (schneiderelectricrepair.com).

Schneider Electric Nigeria

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: