Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
how to change an Array of BYTEs to an Array of INTs or WORDs in the M580 or NOC DIO scanner?
Issue
how to change an Array of BYTEs to an Array of INTs or WORDs in the  M580 or NOC DIO scanner?

Product Line

Unity pro, M580, BMENOC03*1, Control Expert

Resolution

Follow instructions in the attached document.

Schneider Electric Nigeria

Attachment(s)
change an Array of BYTEs to an Array of INTs or WORDs in the M580 or NOC DIO scanner.zip [861.81 KB]