Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the drive ATV930 have direct torque control?
Issue:
Availibility of Direct torque control on the ATV930

Product Line:
ATV930

Environment:
All serial numbers

Cause:
N/A

Resolution:
We do have torque control. There is an algorithm called Direct Torque Control. We don't use that exact algorithm, but it is very similar control.