Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the PDU removable that's included inside the NetShelter CX AR4000MV?
Issue:
A customer wants to replace the PDU in a NetShelter CX Mini.

Product Line:
NetShelter CX

Environment:
AR4000MV, all serial numbers.

Cause:
The brochure doesn't show if the PDU is removable.

Resolution:

The PDU that ships installed inside the AR4000MV is removable.