Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible in Unity pro to force %IW values directly from the Animation Table ?
Issue
Trying to simulate an analog input value.

Product line
Unity Pro , Control Expert

Resolution
No.  To force an analog input you will need to program the WRITE_INPUT_INT block in logic.