Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What level of current flow triggers an SCF3 fault on an ATV61 or ATV71 series drive?

Issue:
ATV61 or ATV71 current flow that triggers an SCF3

Product Line:
ATV61 / ATV71 series

Environment:
All models, All serial numbers

Cause:
Information not available in current literature.

Resolution:
SCF3 faults:
The purpose of this function is to detect a short circuit to the ground at the start-up or while running.

Detection time:
Quick hardware detection (a few μs) . Output current sum > 25% of the current rating of the drive.