Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why I am unable to change the part number of the ATV12 in a SoMove configuration.
Issue:
The Modify Button is not active in the file for an ATV12 in SoMove.
Product Line:
Altivar 12
ATV12
SoMove
Environment:
SoMove
Cause:
The DTM Library prevents the file from being modified.
Resolution:
This issue has been identified and a request has been submitted to have this functionality added.
An update has been requested to resolve this issue.
However, until this has been implemented, there is no possibility of modifying the part number of the ATV12 in a saved file.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: