Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the suffix "EU" indicate on an ATV650 drive?
Issue :
Meaning of the suffix "EU" on an ATV650.

Product Line :
Altivar Process Drive

Environment:
ATV650

Cause :
EU Suffix

Resolution :
E on the part number represents a disconnect switch. U represents UL Type 12 casing.