Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an adjustment to reduce motor oscillation in the ATS48 softstart?
Issue:
Adjustment to reduce motor oscillation in the ATS48.

Product Line:
ATS48

Environment:
All

Cause:
Motor is making a imbalance noise during start and stop.

Resolution:
Stator loss compensation 0 to 90%     default  50%
Parameter active in acceleration phases (and deceleration phases if StY is set to -d-).
In the event of torque oscillations, reduce this parameter gradually until the device is functioning correctly.
Oscillations are most common if the soft starter is connected in motors with excessive slip.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings