Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the ATV320 24Vdc power supply rating?

Article available in these languages: Spanish

Issue:
Planning external uses for the available 24Vdc power supply from the ATV320.

Product line:
ATV320, Altivar 320

Environment:
n/a

Cause:
n/a

Resolution:
The Altivar 320 power supply is rated for 100mA load.  Tolerance of the voltage supply is -15% to +20%.
Note that the logic inputs use 7mA each.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings