Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I install a EStop on an Altistart softstarter?
Issue:
Install EStop on an Altistart softstarts.

Product Line:
ATS48  ATS22  ATS01

Environment:
All series

Cause:
Customer would like the softstart to shut down (stop) on any external fault trips.

Resolution:
Series the external fault contacts (normally closed) with the run / stop command to open on a external fault.