Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to check the warning messages, using SoMove for Altivar Process Drive ATV630 and ATV930?
Issue:
Checking the warning messages using SoMove for the ATV630 and ATV930 drives.

Product Line:
ATV630, ATV930

Environment:
All serial numbers

Cause:
NA

Resolution:
In SoMove software, click on "Diagnostics" and it will display the "Active Warning", "Warning History", and "Warning Groups" under Drive Menu on the left side window.  Select the warning menu that you want to check.