Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a Canopy ?
A Canopy is an overhead roof or else a structure over which a fabric or metal covering is attached, able to provide shade or shelter from weather conditions such as sun, hail, snow and rain.
It guarantees very high protection of the enclosure when used outdoors.