Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the IP degree of protection of the new Harmony + products ?
The global range is IP66, IP67, IP69 and IP69K, find a declaration of conformity where you can find the sub-families which are concerned.

Schneider Electric Nigeria

Attachment(s)
18-006 C&S Harmony d22mm heads IP66, IP67, IP69, IP69K.pdf [44.72 KB]