Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there possibility to parametrize drive in TwinCat without writing application program with sdo read/write ?
The latest versions of the *.xml file (for ATV900, ATV320 and ATV32) allows to configure drive's parameters without creating SDO request in PLC program or to modify the PDO.
The parameters are in “CoE – Online” tab. Picture attached.

Schneider Electric Nigeria

Attachment(s)
rtaImage.jpg [609.2 KB]