{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What tools are needed to set up XVSV series of audio devices?
  • 1 pc of XVSV... product sample.
  • 1 pc of 24Vdc or 110Vac~230Vac power supply.
  • 1 pc of SD card with 4+ GB size. (Kingston, Panasonic, Toshiba, SanDisk and Sony are recommended)
  • 1 pc of PC (x86 or x64) with Windows operating system (WinXP, Win7, Win10).
  • Playlist builder software from SE website.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.