Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you wire and program an ATV630 to replace an ATV58 in a Trane Air Handler?
Issue:
Wondering how do you program an ATV630, to replace an ATV58, in a Trane Air Handler

Product Line:
ATV630

Environment:
All

Cause:
Wiring and programming

Resolution:
A Trane Unit had a board that did the switching for the drive.  If you've wired exactly as before, you only need to Program [Complete settings] > [Command and Reference] > [Ref Freq.1Cfg]  to AI1 and [Complete Settings] [Input/Output] [R2 Configuration] to Drive Running.  Be sure to configure [Simply Start].