Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the main features of PM1130H meter ?

The PM1130H meter supports many features, a few of the features are listed below:

• LED display screen: Intuitive self-guided navigation using four buttons LED
display, with three lines of concurrent values, and load bar that indicates
current loading
• Energy accounting and balancing
• Relay (PM1130H only), alternate source, and RS-485
• THD% for voltage and current, per-phase
• Active, reactive, and apparent energy readings
• Cyber security: The meter enables disabling the RS-485 port through front
panel keys against unauthorized access. This feature can also be used for
toggling between the RTU devices in case of limited availability of nodes in
software system
• Measurement of True PF
You can use the meter as a stand-alone device, but its extensive capabilities are
fully realized when used as part of an energy management system.