Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to use T_M_DIS_STD_CH_STS on BMXDDI3202K?
Question:
How can we use T_M_DIS_STD_CH_STS on BMXDDI3202K in terms of module diagnostic like TRIP, FUSE and Short Circuit?

Answer:
Structure T_M_DIS_STD_CH_STS  is the common structure reserved for DI/DO modules. However, not every bit is used for each module.
Trip function is only used on DO module, so as Short circuit.
Fuse Error could be realized in specific DI module, however it was not realized in DDI 3202K according to R&D.