Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to choose the file extension when a SD card is used for datalogging with M580/M340?
Issue

When creating a file named ‘Test' and write the contents of %MW1-100 to test, what is the file format of 'Test' using SD card and data file? Can this file 'Test' be viewed outside of Unity? Is there a file extension associated with 'Test'?
The help files suggest that after FTP'ing into the SD card we can copy & paste the file into other applications. What applications would that be?

Product Range

M580, SD card

Resolution

When creating a file in Unity pro using SD card and file management library, if the user does not specify the file extension, the result of the created file in a FTP client will be with “no extension”



To associate a file extension, user MUST specify the type of file in Unity pro as show below; the created file can then be opened with appropriate software.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings