Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the available part number prefixes for ION 6200, 7550, 7650, 8650?
Issue
Part numbers and selection might be confusing to customers

Product Line
ION6200
ION7550
ION7650
ION8650

Environment
Product Selection

Cause
Integration of acquired technologies
Branding alignment

Resolution
The S as opposed to an M is used for branding purposes. In fact, the equipment has no differences (other than the first letter of the part number).

The S stands for Square D and is typically used in applications in the United States.

The M stands for Merlin Gerin - a company that was acquired by Schneider Electric in 1992. In 1994, Merlin Gerin and Telemecanique merged into Schneider Electric SA. Merlin Gerin's products, services, and solutions were migrated to the Schneider Electric brand as its Electrical Distribution offer. This international version (part number beginning with an M) is mainly used in applications in Europe and some parts of Canada.

Note: On some datasheets, there is an option for P. This stands for the Power Measurement brand.