Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which drives offer thermal monitoring of the braking resistor?
Issue:
Drive selection for thermal monitoring of the braking resistor.

Product Line:
Altivar drives

Environment:
ATV340, ATV930

Cause:
Braking resistor thermal monitoring

Resolution:
Both the ATV340 and ATV930 offer braking resistor monitoring including thermal state.