Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find documentation on ATV320 drives' physical dimensions?
Issue:
ATV320 dimensions request

Product Line:
Altivar 320, ATEV320 Altivar Machine

Environment:
All

Cause:
Need physical dimensions or drawings.

Resolution:
The best place to find the physical dimensions of any ATV320 drive is in the ATV320 Installation Manual, which can be found by following this link, or see the attached file.
https://www.se.com/ww/en/download/document/NVE41289/

Schneider Electric Nigeria

Attachment(s)
ATV320_installation_manual_EN_NVE41289_05.pdf [4 MB]