Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the IP rating for the Altivar Process Flange Kits?

Issue:
IP rating for VW3A95116.

Product line:
Altivar Process

Environment:
n/a

Cause:
Documentation does not show the IP rating.

Resolution:
The Flange kit is rated as IP40.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.