Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the Tesys T product (LTMR) available with Profinet serial communication option?
Issue:
Is the Tesys T available with Profinet?

Product Line:
LTMR Tesys T

Environment:
All models, All serial numbers.

Cause:
Customer would prefer to use Profinet communication with his Tesys T.  He can use Profibus DP if Profinet is unavailable.

Resolution:
As of 07/2022, Profinet is not available and currently there is no plan to develop Profinet support for the Tesys T LTMR product line.