Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change an ATV630 programming, so that it is a heavy duty rated drive instead of normal duty?

Article available in these languages: Spanish

Issue:
Programming ATV630 for Heavy Duty.

Product Line:
Altivar 630

Environment:
All

Cause:
Rating

Resolution:
Change from normal duty to heavy duty under motor control menu for dual rating.
Change Motor control type to standard from quad.
Note: The rating of the drive does drop by 1 frame size if the drive is heavy duty rated instead of normal duty.