Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
STBNIP2212 Ethernet NIM Web Page Exec. Upgrade to v.1.14.2

Issue
The purpose of this Resolution is to inform Advantys users that the Ethernet NIM Web page firmware has been updated to version 1.14.2.

Product Line
Advantys STB
STBNIP2311

Resolution
Upgrading the STBNIP2212 Ethernet NIM web pages to version 1.14.2 adds support for the following modules:

  • STBACI0320
  • STBACI8320
  • STBACO0220
The attached zip file contains:
  • The web page 'Upgrade Procedure'
  • Upgrade.exe application file
  • Web file: web_files.zr

Please read the 'Upgrade Procedure' in the Attachments before attempting to load the web file.

Schneider Electric Nigeria

Attachment(s)
stbnip2212_web_1142.zip [275.59 KB]