Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ATV320 be set to maintain running speed if the Modbus communication is lost?

Issue:
Maintain running speed on the ATV320 even if the Modbus communication is lost.

Product Line:
ATV320

Environment:
All

Cause:
Configuration

Resolution:
Yes this can be done.
Parameter SLL in the Com Fault Management menu and can be used to modify the behavior of the VFD after a communication interruption: including the option to run at the last commanded frequency or to run at a fixed (fallback) speed.

Care must be taken to ensure safe operation of the equipment...see the drive programming manual for details.
somove

Schneider Electric Nigeria

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings