Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum size of the CoreDB in Easergy T300? What is the maximum number of variables that the T300 can handle?
  • HU250 module includes 1GBit SDRAM memory and each SC150 has 4Mo.
  • The limit of the T300 system comes from the capacity to connect devices (24 SC150 max) upon which the communication could get saturated.
  • However, there are no specific limits concerning the number of variables.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings