Issue:
Description, prerequisites, connecting a PC running EcoStructure Power Commission (EPC) software to Mini USB port
Product Line:
Circuit Breakers
Environment:
Micrologic X, EcoStruxure Power Commission (EPC) Software
Resolution:
Description
From a PC running EPC software, you can access all of the monitoring and control functions of the Micrologic X control unit by connecting a PC directly to the mini USB port of the control unit.
Prerequisites for Using a USB Connection
The prerequisites for establishing a USB connection are:
Connecting a PC Running EPC Software to Mini USB Port
Follow the steps below to connect to the Micrologic X control unit using the mini USB port.
Control Unit Test Mode
The test mode is activated when EPC software is connected to the device through a PC connected to the mini USB port on the Micrologic X control unit and the Force trip button is clicked. For more information, refer to EPC Online Help.
Description, prerequisites, connecting a PC running EcoStructure Power Commission (EPC) software to Mini USB port
Product Line:
Circuit Breakers
Environment:
Micrologic X, EcoStruxure Power Commission (EPC) Software
Resolution:
Description
From a PC running EPC software, you can access all of the monitoring and control functions of the Micrologic X control unit by connecting a PC directly to the mini USB port of the control unit.
Prerequisites for Using a USB Connection
The prerequisites for establishing a USB connection are:
- You must have the USB driver installed on the PC.
- You must have physical access to the Micrologic X control unit to connect the cable directly to the mini USB port of the control unit.
- You must have a USB cable (reference LV850067SP) to connect the USB port of the PC to the mini USB port of the Micrologic X control unit.
Connecting a PC Running EPC Software to Mini USB Port
Follow the steps below to connect to the Micrologic X control unit using the mini USB port.
- Connect your PC to the mini USB port of the Micrologic X control unit using a cable with reference LV850067SP. The PC provides power to the Micrologic X control unit if necessary.
- Start EPC software on the PC and log in.
- On the EPC home page, connect to the Micrologic X control unit. There are different ways to connect EPC software to the Micrologic X control unit, depending on whether it is the first connection and how the device was discovered. For more information, refer to EPC Online Help.
- With EPC software connected to the Micrologic X control unit you have access to all functions of the software.
Control Unit Test Mode
The test mode is activated when EPC software is connected to the device through a PC connected to the mini USB port on the Micrologic X control unit and the Force trip button is clicked. For more information, refer to EPC Online Help.
Released for: Schneider Electric Nigeria


Need help?
- Product Selector- Quickly and easily find the right products and accessories for your applications. 
- Get a Quote- Start your sales enquiry online and an expert will connect with you. 
- Where to buy?- Easily find the nearest Schneider Electric distributor in your location. 
- Help Centre- Find support resources for all your needs, in one place.