How can we help you today?

Unity Pro wrong behaviour due to cybersecurity protection

Goals and Symptoms

Operating with Unity Pro offline or online connected to PLC, some functionality may not end properly.

Facts and changes

On the machine where Unity Pro is installed, the antivirus is scanning files and does not allow Unity Pro to use some temporary files needed for the normal execution of Unity Pro.

Causes and Fixes

To workaround this situation we suggest to adjust antivirus to not scan the UnityProTemp folder.
In your antivirus add an exception for the following folder:
C:\UnityProTemp\%userid%
Next improvement will be in Unity Pro V14.