Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Making a switch in Vijeo Designer that remains down while the bit is high

In Vijeo Designer, we must make use of two objects to animate a switch that stays down while the bit is high and that is also able to reset the bit when touching it.

We make use of:
1) A radio button (to set the bit and to stay down when the bit is high)
2) An invisible switch to be used to reset the bit. The switch has a visibility condition to only appear when the bit is high.

Please see the following video for a demonstration of this procedure:

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Attachment(s)
DownStateSwitch.zip [17.51 KB]