Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why Node-red embedded with Ecostruxure Augmented Operator Advisor stop few second after starting?
Symptom
After few second, you can see that Node-red stop working

How to diagnostic
When you start AOA, there is one MS-dos windows with a lot of information
ms doc description
In this exemple, you can see that the problem occur after flow starting and after more details about which flow create this error

How to solve the problem
This flow error avoid to start Node-red.
So, we will see how to restart with the previous working flow

Go to …Schneider-electric \ Ecostruxure Augmented Operator Advisor \ Node-red \ node-red home
file to update
In this folder you can see the current flow and also the last backup
The propose is to reuse the backup (the last working flow) and delete or rename the current flow (the flow creating node-red crash)
  1. Change the name or remove the flow named flow_W7FRN05933L.json
  2. Change the name of the backup .flow_W7FRN05933L.json.backup to  flow_W7FRN05933L.json
  3. Restart node-red