Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a function block in SoMachine V4.3 to extract the bits of a words?

Issue:
Looking for a way to extract or set a bit within a word.

Product Line:
SoMachine, EcoStruxure Machine Expert

Resolution:
Sometimes it becomes necessary to extract or set a bit within a word.

Those function blocks can be found under the Functionblocks section under Bit/Bytes Functions of SoMachine V4.3.  Or you can simply type in WORD_AS_BIT or BIT_AS_WORD on the empty box.

The block also have to have a unique instance name.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Attachment(s)
W2B.jpg [36.25 KB]
W2B_FB.jpg [120.54 KB]