Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I transfer programming from an ATV32 or ATV320 while function blocks are running?

Article available in these languages: Spanish

Issue:
Can I transfer files from an ATV320 while function blocks are running?

Product Line:
Altivar 32, Altivar 320

Environment:
All

Cause:
Need to transfer programming from one drive to another

Resolution:
No, programming cannot be saved or transferred while function blocks are running.
The function block programming must be stopped before the transfer.