Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find details on the ATV320 Underload Alarm?
Issue:
ATV320 Underload Alarm details.

Product Line:
Altivar 320

Environment:
All

Cause:
Parameter clarification

Resolution:
The Alarm ULA ( underLoad Alarm) is operational, when you use detection fault function " Process UnderLoad " and  "Underlaod management" UDL is assigned to NO.
Otherwise the drive trips in fault ULF and follow ramp, freewheel , fast stop.

Now if UDL=NO, and you assigned for example R1= ULA. When the motor torque is on Underload Zone (see picture below) during the delay set on "Underload detection time delay"  ULT, the relay become active, and motor still in RUN (so no fault only alarm actif-> relay actif). The relay becomes inactive when the motor is stopped or leave the underload zone.

Underload torque

For more information about Underload function, please see document attached (extract of programming manual).

Schneider Electric Nigeria

Attachment(s)
ATV320_UnderLoadManagement.pdf [70.5 KB]