Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I save and send a recipe automatically in EcoStruxure Operator Terminal Expert (formerly known as Vijeo XD V3.0)?

Issue:
Looking for a way to save and send a recipe automatically

Product Line:
HMISTO705, HMISTO715, HMIST735, EcoStruxure Operator Terminal Expert

Resolution:
The HMISTO705, HMISTO715 and HMISTO735 does not have the ability to retain internal variable on a power cycle.

As a workaround it is possible to mimic this behavior using a recipe. In the script seen below, when the Runtime Starts, a recipe is loaded and the same recipe is saved every 15 seconds.
Blockly script

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings