How can we help you today?

How do we have to understand the parameter "maximum overload Voltage +-30VDC" in a the module BMEAH? Does it means +-30VDC in absolute or +-30 VDC in measuring loop 24VDC...?

The customer needs to get a clarification of the parameter „"maximum overload Voltage +-30 VDC" delivered for the module BMEAHI0812. The customer could think that it means +-30VDC in absolute or +-30 VDC in measuring loop 24VDC meaning 24VDC +-30VDC means 24+30 = 54VDC as maximum overload voltage.

The answer is +-30VDC, not +-54VDC.

Schneider Electric Nigeria