Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the ATV212, SFLEX and SFD part numbers?
Issue :
Wants to know the difference between the ATV212, S-FLEX and SFD part numbers?

Product Line :
Altivar Machines, Altivar 212, S-Flex

Environment :
All models and serial numbers

Resolution :
S-Flex is the enclosed version of the ATV212 part number. S-Flex part number begin with SFD212, and the end of this part number will indicate HP, Voltage and modifications.