Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Please suggest solution for E20 error in ATV212 Drive?
Hello,

If you are facing E20 fault during declaration, we suggest the below

1. Do factory reset of the parameters typ = 3 and enter. It will change the parameter setting to factory default value.

2. Set the motor nameplate parameters in motor control menu and do a auto-tuning F400 = 2 and give start command. F400 will change to 0 automatically after successful completion of auto-tuning.

If the problem is not solved after above implementing above two suggestions, The E-20 is an over toque boost fault this is similar to a OBF in your case.

Try the following action:

Set the parameter F418 and F419 - follow the programming manual to fine-tune(increase or decrease to optimize) this parameters. Because at first it seems your inertia is very heavy that may be the root cause of your E-20, hence you will have to change this parameter.
if it doesn't work
pt=3
Tuning
put AU1 to 1
increase the DEC ramp.
and modify F418 and F419.
We hope it will help to optimize the torque boost and solve the problem.