Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is an ASF fault on an ATV320 drive?
Issue:
Getting an ASF fault on an ATV320 drive

Product Line:
ATV320 drives

Environment:
ASF faults

Cause:
Occurs during the phase-shift angle measurement, if the motor phase is disconnected or it the motor inductance is too high.

Resolution:
Check the motor phases and the maximum current allowed by the drive.