Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to start and stop the PowerChute Agent service

Issue:
How to start and stop the PowerChute Agent service


Product:
PowerChute Business Edition v9.5 and higher
PowerChute Serial Shutdown v1.x


Environment:

All supported operating systems


Solution:

Follow the steps detailed below to start and stop the Agent service.


Windows

For Windows 11 open File Explorer and enter Control Panel\All Control Panel Items\Windows Tools\Services

For older versions of Windows, navigate to Windows Services under Administrative Tools in the Control Panel and locate the PowerChute Business Edition Agent service (APC PBE Agent), PowerChute Serial Shutdown Agent service (PowerChute Serial Shutdown)

For PowerChute Business Edition
To manually start the Agent, right-click on APC PBE Agent and select Start.
To manually stop the Agent, right-click on APC PBE Agent and select Stop.


For PowerChute Serial Shutdown
To manually start the Agent, right-click on PowerChute Serial Shutdown and select Start.
To manually stop the Agent, right-click on PowerChute Serial Shutdown and select Stop.
To manually restart the Agent, right-click on PowerChute Serial Shutdown and select Restart.

Using Command Prompt, Open Command Prompt as an administrator
Enter
net start apcpbeagent (to start the service)
net stop apcpbeagent (to stop the service)

Using PowerShell open as an administrator
Enter
Stop-Service APCPBEAGENT
Start-Service APCPBEAGENT
Restart-Service APCPBEAGENT

Linux

To manually start or stop the PowerChute Business Edition or PowerChute Serial Shutdown service, enter the following command in a command/terminal window.

NOTE: You must have administrator privileges to execute these commands.

/etc/init.d/PBEAgent start (to start the service)
/etc/init.d/PBEAgent stop (to stop the service)

RHEL and SUSE
service pbeagent start (to start the service)
service pbeagent stop (to stop the service)

(or)

systemctl start PBEAgent.service (to start the service)
systemctl stop PBEAgent.service (to stop the service)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings