Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you clear fault code EPF1 on the Altivar ATV61 and ATV71 drives?

Issue:
Clearing EPF1 on the Altivar ATV61 and ATV71

Product Line:
ATV61
ATV71

Environment:
ALL

Cause:
Wiring / Programming

Resolution:
EPF1 indicates an external device has triggered the drive to trip.
d

This is normally an external signal connected to a logic input on the drive and programmed in Menu 1.8: Fault Management.
s
A Power Cycle is required to reset the error, once the correct signal is restored.
Commanding a Fault reset via the logic inputs, the keypad, or over serial communication will not clear EPF1.

Schneider Electric Nigeria

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: