Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What do I do when I see Error 1392 "When using logged variable values, assign the variable to a data logging group." in the Vijeo Designer Feedback Zone?

Issue

Error 1392 "When using logged variable values, assign the variable to a data logging group." appears when a Vijeo Designer HMI project is built.

Product Line

Vijeo Designer v4.5+

Environment

Windows 7, Windows 10

Cause

When Error 1392 "When using logged variable values, assign the variable to a data logging group." appears, it means that a Variable designated for logging that was mandatory is no longer assigned . In working with data logging, you must assign the variable to a data logging group, which contains a set of properties that specifies the data collection method and data storage details for a variable.

Resolution

Assign the variable to a data logging group using the Data Details tab in the Variable Properties dialog box or in the Variable node's Logging Group column.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings