{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does a P or H symbolize in an ATV12 drive part number?
Issue:
ATV12 part number P or H meaning

Product Line:
Altivar 12

Environment:
All

Cause:
Part number

Resolution:
The ATV12 drives are available as H or P version. Part numbers with H are drives with a standard heatsink on the back of the drive.
Ex: ATV12H037M2 has a heatsink. Replace the H with P for drives without a heatsink. Instead of a heatsink, these drives have a smooth, flat metal back that can be mounted to a thermally conductive machine surface.
The P version is available up to 1HP for single phase input voltage and up 5HP for three phase input voltage.

H version: ATV12H P version: ATV12 P

Refer to Installation Manual BBV28587 for further details: https://www.se.com/ww/en/download/document/BBV28587/

Schneider Electric Nigeria